SLOSE70 December 2020 DRV8434S
PRODUCTION DATA
Smart tune Ripple Control operates by setting an IVALLEY level along with the ITRIP level. When the current level reaches ITRIP, instead of entering slow decay until the tOFF time expires, the driver enters slow decay until IVALLEY is reached. Slow decay operates similar to slow/slow decay where both low-side MOSFETs are turned on allowing the current to recirculate. In this mode, tOFF is variable depending on the current level and operating parameters.
The ripple current in this decay mode is programmed by the RC_RIPPLE[1:0] bits. The ripple current is dependent on the ITRIP of a particular microstep level.
RC_RIPPLE | Current Ripple at a specific microstep level |
---|---|
00b | 19mA + 1% of ITRIP |
01b | 19mA + 2% of ITRIP |
10b | 19mA + 4% of ITRIP |
11b | 19mA + 6% of ITRIP |
This ripple control method allows much tighter regulation of the current level increasing motor efficiency and system performance. Smart tune Ripple Control can be used in systems that can tolerate a variable off-time regulation scheme to achieve low current ripple with current regulation. Select a lowest possible ripple current setting that ensures the PWM frequency is above the audible range.