SLOSE98A December 2022 – September 2023 DRV8461
PRODUCTION DATA
When operating with the SPI interface, the DRV8461 supports an internal 3.3 V reference voltage. This internal reference can be enabled by writing 1b to the VREF_INT_EN bit. The voltage on the VREF pin will be ignored in that case, and the VREF pin can be left open or connected to ground.
The full-scale current and the holding current will be calculated as shown in Equation 14 and Equation 5 -
Using the internal 3.3 V as reference will save BOM cost by eliminating the two resistors connected to the VREF pin.