SLVS912J January 2009 – January 2016 DRV8821
PRODUCTION DATA.
For details about how to design the PCB, refer to TI application report, PowerPAD™ Thermally Enhanced Package SLMA002 and TI application brief, PowerPAD™ Made Easy, SLMA004 available at www.ti.com.
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
PowerPAD, E2E are trademarks of Texas Instruments.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.