SLVSE65C July 2018 – December 2023 DRV8847
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Now, the pull up current of ISC (155.56-µA) is flowing from the internal regulator (AVDD), therefore the voltage at the positive terminal of OL1_HS comparator (which is also the OUT1 node) is calculated as,
using Equation 22, the VOL1_HS(+) is calculated as,
This voltage, if compared with 2.3-V (VOL_HS) sets the OL1_HS comparator output to "1".