SLVSGF6A May 2023 – October 2023 DRV8849
PRODUCTION DATA
The current through the motor windings is regulated by an adjustable, off-time PWM current-regulation circuit. When an H-bridge is enabled, current rises through the winding at a rate dependent on the DC voltage, inductance of the winding, and the magnitude of the back EMF present. When the current hits the current regulation threshold (as shown in Figure 8-6, Item 1), the bridge enters a decay mode determined by the DECAY pin setting to decrease the current. After the off-time expires, the bridge is re-enabled, starting another PWM cycle.
Once the chopping current threshold is reached, the H-bridge can operate in two different states, fast decay or slow decay.
In fast decay mode, as soon as the PWM chopping current level is reached, the H-bridge reverses state by switching on the opposite arm MOSFETs to allow the winding current to flow in the opposite direction. As the winding current approaches zero, the H-bridge is disabled to prevent further reverse current flow. Fast decay mode is shown in Figure 8-6, item 3.
In slow decay mode, the winding current is re-circulated by enabling both low-side MOSFETs in the H-bridge. This is shown in Figure 8-6, Item 2.
The PWM regulation current is set by a comparator which monitors the voltage across the current sense MOSFETs in parallel with the low-side power MOSFETs. The current sense MOSFETs are biased with a reference current that is the output of a current-mode sine-weighted DAC whose full-scale reference current is set by the voltage at the VREF pins.
The full-scale regulation current (IFS) can be calculated as -
IFS (A) = VREFx (V) / KV (V/A) = VREFx (V) / 2.2 (V/A).
The decay mode of the DRV8849 is selected by the DECAY pins as shown in Table 8-6. The decay modes can not be changed on the fly - they are latched after power-up.
DECAYx | DECAY MODE |
---|---|
0 | Smart tune Ripple Control |
1 | Smart tune Dynamic Decay, 16 μs OFF time |
Hi-Z | Smart tune Dynamic Decay, 32 μs OFF time |
330k to GND | Smart tune Dynamic Decay, 8 μs OFF time |