SLVSD18C June 2015 – August 2017 DRV8880
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
During fast decay, the polarity of the H-bridge is reversed. The H-bridge will be turned off as current approaches zero in order to prevent current flow in the reverse direction. In this mode, fast decay only occurs during decreasing current. Slow decay is used for increasing current.
Fast decay exhibits the highest current ripple of the decay modes for a given tOFF. Transition time on decreasing current steps is much faster than slow decay since the current is allowed to decrease much faster.