SLVSD19A June 2015 – July 2015 DRV8881
PRODUCTION DATA.
The peak current in a motor driver is limited by the overcurrent protection trip threshold IOCP. The peak current describes any transient duration current pulse, for example when charging capacitance, when the overall duty cycle is very low. In general the minimum value of IOCP specifies the peak current rating of the motor driver. For the DRV8881, the peak current rating is 2.5 A per bridge.