SLVSDO1C January 2017 – March 2020 DRV8886AT
PRODUCTION DATA.
In a stepper motor, the full-scale current (IFS) is the maximum current driven through either winding. This quantity depends on the RREF resistor and the TRQ setting. During stepping, IFS defines the current chopping threshold (ITRIP) for the maximum current step.
NOTE
The IFS current must also follow Equation 8 to avoid saturating the motor. VM is the motor supply voltage, and RL is the motor winding resistance.