SLVSEE9D April 2020 – April 2021 DRV8889-Q1
PRODUCTION DATA
The peak current in a stepper driver is limited by the overcurrent protection trip threshold IOCP. The peak current describes any transient duration current pulse, for example when charging capacitance, when the overall duty cycle is very low. In general the minimum value of IOCP specifies the peak current rating of the stepper motor driver.
The peak current rating of the device is 2.4 A per bridge.