SNLS397D October 2011 – April 2015 DS110DF410
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The DS110DF410 is a 4-channel retimer that supports many different data rates and application spaces.
The following sections describe the typical use cases and common implementation practices.
Figure 6 shows a typical system implementation, where the DS110DF410 is used both on the backplane and port side.
This section lists some critical areas for high speed printed circuit board design consideration and study.
To begin the design process, determine the following:
Figure 7 shows a typical output eye diagram for the DS110DF410 operating at 10.3125 Gbps with default VOD of 600mVp-p and de-emphasis setting of –2dB.
Figure 8 shows an example of Tx de-emphasis for a DS110DF410 operating at 10.3125 Gbps. In this example, the high speed output is configured for 600mVp-p VOD and de-emphasis is set to –4.5dB. An 8T pattern is used to evaluate the driver, which consists of 0xFF00.