As with any high-speed design, there are many
factors which influence the overall performance. The following list indicates
critical areas for consideration during design.
- Use 85 Ω impedance traces
when interfacing with PCIe CEM connectors. Length matching on the P and N
traces should be done on the single-end segments of the differential
pair.
- Use a uniform trace width and
trace spacing for differential pairs.
- Back-drill connector vias and
signal vias to minimize stub length.
- Use reference plane vias to
ensure a low inductance path for the return current.