The design procedure for backplane/mid-plane applications is as follows:
- Determine the total number of channels on the board which require a DS250DF230 for signal conditioning. This will dictate the total number of DS250DF230 devices required for the board. It is generally recommended that channels with similar total insertion loss on the board be grouped together in the same DS250DF230 device. This will simplify the device settings, as similar loss channels generally use similar settings.
- Determine the maximum current draw required for all DS250DF230 retimers. This may impact the selection of the regulator for the 2.5-V supply rail. To calculate the maximum current draw, multiply the maximum transient power supply current by the total number of DS250DF230 devices.
- Determine the maximum operational power consumption for the purpose of thermal analysis. There are two ways to approach this calculation:
- Maximum mission-mode operational power consumption is when all channels are locked and re-transmitting the data which is received. PRBS pattern checkers/generators are not used in this mode because normal traffic cannot be checked with a PRBS checker. For this calculation, multiply the worst-case power consumption in mission mode by the total number of DS250DF230 devices.
- Maximum debug-mode operational power consumption is when all channels are locked and re-transmitting the data which is received. At the same time, some channels’ PRBS checkers or generators may be enabled. For this calculation, multiply the worst-case power consumption in debug mode by the total number of DS250DF230 devices.
- Determine the SMBus address scheme needed to uniquely address each DS250DF230 device on the board, depending on the total number of devices identified in step 2. Each DS250DF230 can be strapped with one of 16 unique SMBus addresses. If there are more DS250DF230 devices on the board than the number of unique SMBus addresses which can be assigned, then use an I2C expander like the TCA/PCA family of I2C/SMBus switches and multiplexers to split up the SMBus into multiple busses.
- Determine if the device will be configured from EEPROM (SMBus Master Mode) or from the system I2C bus (SMBus Slave Mode).
- If SMBus Master Mode will be used, provisions must be made for an EEPROM on the
board with 8-bit SMBus address 0xA0. Refer to SMBus Master Mode for more details on SMBus Master Mode including
EEPROM size requirements.
- If SMBus Slave Mode will be used for all device configurations, an EEPROM is not needed.
- Make provisions in the schematic and layout for standard decoupling capacitors
between the device VDD supply and GND. Refer to the pin function description in Pin Configuration and Functions for more details.
- Make provisions in the schematic and layout for a
30.72-MHz (±100 ppm) or 25-MHz (±100 ppm) single-ended CMOS clock. Each
DS250DF230 retimer buffers the clock on the CAL_CLK_IN pin and presents the
buffered clock on the CAL_CLK_OUT pin. This allows multiple (up to 20) retimers’
calibration clocks to be daisy chained to avoid the need for multiple
oscillators on the board. If the oscillator used on the board has a 2.5-V CMOS
output, then no AC-coupling capacitor or resistor ladder is required at the
input to CAL_CLK_IN. No AC coupling or resistor ladder is needed between one
retimer’s CAL_CLK_OUT output and the next retimer’s CAL_CLK_IN input. The final
retimer’s CAL_CLK_OUT output can be left floating.
- Connect the INT_N open-drain output to an FPGA or CPU if interrupt monitoring is desired. Note that multiple retimers’ INT_N outputs can be connected together because this is an open-drain output. The common INT_N net must be pulled high.
- If the application requires initial CDR lock acquisition at the ambient
temperature extremes defined in Recommended Operating Conditions, take care to ensure the operating
junction temperature is met as well as the CDR stay-in-lock junction temperature range
defined in Electrical
Characteristics. For example, if initial CDR lock acquisition occurs at an
junction temperature of 110 °C, then maintaining CDR lock would require the junction
temperature on DS250DF230 to be kept above (110°C - TEMPLOCK-).