4 Revision History
Changes from Revision A (December 2020) to Revision B (September 2023)
- Fixed spelling errors and minor format issues throughout the
documentGo
- Removed "Port Replication Mode" from the list of device
featuresGo
- Fixed spelling errors and minor format issues throughout the
document Go
- Updated I2C pull-up resistor recommendationsGo
- Updated Legend for Pin Functions TableGo
- Removed the tCLK-MISS specification from the CSI-2 Timing Specifications tableGo
- Updated Timing Diagrams section figure titles to align with the figuresGo
- Removed obstructions in CSI-2 General Frame Format figure to make text clearerGo
- Updated the title of the section with timing figures to Timing DiagramsGo
- Clarified the clock speed and the configuration settings of
non-synchronous clock modeGo
- Added information about YUV supportGo
- Added clarification that MODE pin
option 0 straps the device to CSI-2
Non-Synchronous back channel and MODE pin option 4
straps the device to CSI-2 Synchronous back
channelGo
- Changed I2C terminology to "Controller" and
"Target"Go
- Added a channel requirements section to the datasheetGo
- Fixed spelling errors throughout the documentGo
- Fixed spelling errors throughout the documentGo
- Added information about YUV supportGo
- Removed mention of older siliconGo
- Removed CSI-2 Transmitter Frequency script example for unsupported
CSI-2 portGo
- Added cross-links in the CSI-2 Output Bandwidth section to relevant figures in the Timing Diagrams sectionGo
- Fixed spelling errors throughout the documentGo
- Added a sentence to clarify that VI2C must match the voltage
applied to VDDIOGo
- Reworded the Serial Control Bus section to reference VI2C instead
of VDDIOGo
- Added register addresses for the RX Port ID
registersGo
- Removed information suggesting that the Rx Port intended for messaging must always be selected with Register 0x4C when communicating with a remote target deviceGo
- Corrected the total number of TargetID and Target Alias pairs of registers for the
deviceGo
- Clarified that the write enable bit in register 0x4C needs to be set before configuring remote target addressesGo
- Added additional information about how to configure a broadcast write to remote devicesGo
- Removed unnecessary register writes in the Code Example for
Broadcast WriteGo
- Updated the I2C Controller Proxy descriptionGo
- Fixed register address errors in the Typical I2C Timing Register
Settings tableGo
- Removed details about the internal reference clockGo
- Corrected typo that mentions two CSI-2 Transmit ports in the Interrupt
Support sectionGo
- Replaced CABLE_FAULT with NO_FPD3_CLK in the interrupt readback
example script to match the register bit nameGo
- Clarified instructions for how to configure Pattern Generation on
the CSI-2 PortGo
- Removed all RESERVED registers from the datasheetGo
- Updated description of registers 0x10-0x17 to remove mention of unsupported
CSI-2 TX PortGo
- RESERVED register bits 0x20[3:0] that have no customer use
caseGo
- RESERVED register bit 0x32[4] that has no customer use caseGo
- Made register bits 0x34[5:4] public and updated the description of register bit 0x34[1]Go
- Corrected a bit description typo for bit 4 of register 0x4AGo
- Updated the description of register bit 0x4E[1] to clarify
functionalityGo
- Updated the description sections of registers 0x51-0x54Go
- Fixed typos in the description for registers 0x90-0x97Go
- Removed RESERVED indirect register pages in the description of register bits
0xB0[5:2]Go
- Made register 0xB6 publicGo
- Updated the bit description of 0xB9[3:0]Go
- Updated the name of Indirect Register Page 0 to PATGEN_AND_CSI-2Go
- Updated the PoC descriptionGo
- Updated all typical connection diagrams to include a reference to App Note
SLVA689Go
- Added clarification for the recommended ferrite bead characteristics on the power supply railsGo
- Removed optional 10 kΩ pulldown resistor on Pin 4 in the Typical Connection
DiagramGo
- Added clarification for the NC pin connections in the Typical Connection
DiagramGo
- Updated MIPI CSI-2 D-PHY layout recommendationsGo
Changes from Revision * (August 2018) to Revision A (December 2020)
- Added feature bullet Functional Safety Capable Go
- Changed ESD HBM other pins to +/- 3000VGo