SNOSCZ4A April 2015 – October 2024 FDC1004-Q1
PRODUCTION DATA
Make sure the liquid level measurement is independent of the liquid, which can be achieved using the 3-electrode design described above. Moreover, make sure the sensor is immune to environmental interferences such as a human body, other objects, or EMI. This can be achieved by shielding the side of the sensor which does not face the container.