SBOS781E March 2016 – May 2021 INA199-Q1
PRODUCTION DATA
The device can be configured to monitor current flowing in one direction (unidirectional) or in both directions (bidirectional), depending on how the REF pin is configured. The most common case is unidirectional where the output is set to ground when current is not flowing by connecting the REF pin to ground; see Figure 9-7. When the input signal increases, the output voltage at the OUT pin increases.