SBOS469H April 2009 – October 2023 INA199
PRODUCTION DATA
The device can be configured to monitor current flowing in one direction (unidirectional) or in both directions (bidirectional) depending on how the REF pin is configured. The most common case is unidirectional where the output is set to ground when no current is flowing by connecting the REF pin to ground, as shown in Figure 8-1. When the input signal increases, the output voltage at the OUT pin increases.