SBOS805C July 2016 – September 2023 INA250-Q1
PRODUCTION DATA
Occasionally, the need may arise to confirm that the current into a load is identical to the current coming out of a load, such as when performing diagnostic testing or fault detection. This procedure requires precision current differencing. This method is the same as current summing, except that the two amplifiers have the respective inputs connected opposite of each other. Under normal operating conditions, the final output is close to the reference value and proportional to any current difference. Figure 8-5 is an example of two INA250-Q1 devices connected for current differencing.