SBOS999A March 2022 – October 2022 INA851
PRODUCTION DATA
There are two modes of operation for the circuit shown in Figure 9-3: current input and voltage input. This design requires R1 >> R2 >> R3. Given this relationship, the following equation calculates the current input mode transfer function.
where
The following equation shows the transfer function for the voltage input mode:
where
The voltages on the output pins of the INA851 follow the relationships in Equation 8 and Equation 9.
R1 sets the input impedance of the voltage input mode. The minimum typical input impedance is 100 kΩ. The R1 value is 100 kΩ because increasing the R1 value also increases noise. The value of R3 must be extremely small compared to R1 and R2. A 20‑Ω value is selected for R3 because that resistance value is much smaller than R1 and yields an input voltage of ±400 mV when operated in current mode (±20 mA).
Use Equation 10 to calculate R2 given VDIFF = ±400 mV, VIN = ±10 V, and R1 = 100 kΩ.
The value obtained from Equation 10 is not a standard 0.1% value; therefore, 4.17 kΩ is selected. R1 and R2 also use 0.1% tolerance resistors to minimize error.
Use Equation 11 to calculate the gain of the instrumentation amplifier.
Equation 12 calculates the gain-setting resistor value using the INA851 gain equation for GOUT = 1 V/V (Equation 1).
Use a standard 0.1% resistor value of 530 Ω for this design.
The ADS8920B is selected because of the differential input, 1-MSPS sampling rate, and integrated reference buffer. Implement the antialiasing R-C-R filter using two 47.4-Ω resistors, a COG or NPO-type 510-pF differential capacitor, and two ceramic 51-pF common-mode capacitors. The REF5050 is selected to create a 5-V reference voltage for the ADC. Use well-matched precision resistors to create a voltage divider that generates a stable 2.5-V VOCM reference. Connect the VCLAMP+ and VCLAMP− pins of the INA851 to the supplies of the ADC to protect against overdrive damage in the event of a fault. Consider implementing a TVS diode from the ADC supply to GND for additional protection, and include 100-nF decoupling capacitors between the amplifier and ADC supplies and GND.