SBOS999A March 2022 – October 2022 INA851
PRODUCTION DATA
An output noise calculation helps design a low-noise circuit to drive high-precision ADC applications and optimize the signal-to-noise ratio (SNR).
Figure 8-14 shows a simplified noise model for the INA851. The eNO noise refers to the input resistor network of the FDA. This term incorporates the thermal noise of the internal feedback resistors, and the interaction of the internal current noise density of the output stage with the internal feedback resistors.
The internal feedback resistor network is considered in the eNO specification; therefore, the calculation of the total input-referred noise, eN(RTI), is simplified to the following equation:
The total output-referred noise, eN(RTO), multiplies directly by the output stage gain, GOUT, by GOUT = 0.2 V/V or GOUT = 1 V/V respectively, as shown in the following equation: