SWRS311 December 2024 IWRL6432W
PRODUCTION DATA
The following the system topologies are supported.
In Topology 1: Autonomous mode, the IWRL6432W can be used as full sensor along with M4F application processor. In this case the internal application processor does all the processing and interrupts the host processor to communicate to take action based on the sensor data. Most of the processing happens on the internal MCU of the IWRL6432W chip and only high level desired results are communicated to external host. In this topology MIPS, processing capability on the external MCU is relaxed and very low cost and low power MCU can be used.
In Topology 2: Peripheral mode, the IWRL6432W is controlled by an external MCU and most of the processing is done on an external MCU. In this case, computational and power requirements are higher and the external MCU stays active most of the time.