When the LDC3114 is active (in
either Normal Power Mode or Low Power Mode), use Equation 15 to determine the current:
Equation 15. where
- IACTIVEn is the supply
current in mA during active sampling
- RPn is the sensor
parallel resonant impedance in kΩ
- fSENSORn is the
sensor frequency in MHz
- n is the channel index, that is, n
= 0, 1, 2, or 3 for LDC3114
The LDC3114 is only actively
sampling the enabled channels during a fraction of the scan window. Equation 16 determines the average supply
current:
Equation 16. where
- IDD is the average supply current in
mA
- tSCAN is the scan window (set
by the scan rate) in ms
- IACTIVEn is the supply
current when the device is active as defined by Equation 15
- tSAMPLE is the button sampling window in ms