SNOSDD0 December 2021 LDC3114
PRODUCTION DATA
The LDC3114 automatically tracks slow changes in the baseline signal and compensates for environmental drifts and variations. The baseline tracking is only applicable for the button algorithm mode and not for raw data access mode. See Section 7.3.1 for details. In Normal Power Mode, use Equation 11 to determine the effective baseline increment per scan cycle (BINCNP):
where:
In Low Power Mode, use Equation 12 to determine the effective baseline increment per scan cycle (BINCLP):
where:
As a result of baseline tracking, a button press with a constant force only lasts for a finite amount of time. Equation 13 defines the duration of a button press (DATAn > ThresholdON).
where:
The baseline tracking for a particular channel can be paused when the channel output is asserted. This is achieved by setting the corresponding BTPAUSE bit in Register BTPAUSE_MAXWIN (Address 0x16) to b1.
If DATAn is negative, the tracking speed will be scaled by the fast tracking factor as specified in Registers FTF0 (Address 0x25) , FTF1_2 (Address 0x28), or FTF3 (Address 0x2B). Table 8-2 shows the scaling factors for various FTFn settings.
FTFn Setting | Fast Tracking Factor |
---|---|
b00 | 1 |
b01 | 4 |
b10 | 8 |
b11 | 16 |