SNOSDI7 December 2023 LDC5071-Q1
PRODUCTION DATA
In some scenarios, it may be desirable to connect to a single-ended ADC. This will reduce the number of wires leaving the LDC5071-Q1 sensor board, but it will also reduce the dynamic range, SNR, and noise immunity. If it is possible to use the LDC5071-Q1 in differential mode, then that should be the first choice for the system designer. Refer to Table 7-1 for component values. If single-ended mode must be used, follow these guidelines: