SNOSDI7 December 2023 LDC5071-Q1
PRODUCTION DATA
In the DIAGNOSTICS state, the LDC5071-Q1 undergoes a number of self-diagnostics and checks to confirm whether or not the device is functioning as expected and that all sensors are properly connected. See Diagnostics for more information.
The device transitions to the DIAGNOSTICS state from one of the following:
The device transitions from the DIAGNOSTICS state to one of the following: