SNVS729F September 2011 – August 2014 LM10506
PRODUCTION DATA.
The LM10506 device provides 4 regulated outputs from 3 step-down switching regulators and one linear regulator. The regulated outputs are achieved using a minimum of external components. To support low load conditions within an application the device may be placed in a low power mode - STANDBY.
A 4-wire SPI interface may be used to reconfigure the device outputs and return an indication of output status. A separate device output provides an Interrupt signal when the device status changes. All programmed settings may be returned to default state via a RESET input.
REGULATOR | VOUT if H/L=HIGH (B2, B3) |
VOUT if H/L=LOW (B2, B3) |
VOUT if STANDBY=HIGH (STANDBY MODE) |
VOUT | MAXIMUM OUTPUT CURRENT | TYPICAL APPLICATION | COMMENTS |
---|---|---|---|---|---|---|---|
Buck 1(1) | 3 V | 3 V | Off | 1.1 V to 3.6 V; 50-mV steps |
1.3 A | VCC | Flash |
Buck 2(1) | 3 V | 1.8 V | Off | 1.1 V to 3.6 V; 50-mV steps |
400 mA | VCCQ | Interface |
Buck 3(1) | 1.2 V | 1 V | VNOM - 7% | 0.7 V to 1.335 V; 5-mV steps |
600 mA | VCORE | Core |
LDO | 3.2 V | 3.2 V | 3.2 V | N/A | 100 mA | VHOST controller | Reference for Digital |
REGULATOR | VOUT if H/L=HIGH (B2, B3) |
VOUT if H/L=LOW (B2, B3) |
VOUT if STANDBY=HIGH (STANDBY MODE) |
VOUT | MAXIMUM OUTPUT CURRENT | TYPICAL APPLICATION | COMMENTS |
---|---|---|---|---|---|---|---|
Buck 1(1) | 3 V | 3 V | Off | 1.1 V to 3.6 V; 50-mV steps |
1.3 A | VCC | Flash |
Buck 2(1) | 2 V | 1.8 V | Off | 1.1 V to 3.6 V; 50-mV steps |
400 mA | VCCQ | Interface |
Buck 3(1) | 1.2 V | 1 V | VNOM - 7% | 0.7 V to 1.335 V; 5-mV steps |
600 mA | VCORE | Core |
LDO | 3.2 V | 3.2 V | 3.2 V | N/A | 100 mA | VHOST controller | Reference for Digital |
VIN, VIN_B1, VIN_B2, and VIN_B3 must all be connected to the same power source.
Ensure that the device is in a low power mode before entering Standby and throughout the Standby phase. In Standby mode the device is in a low power mode in which all internal clocks are turned off to conserve power and Buck 3 will only operate in PFM mode. While limited to PFM mode the loading on Buck 3 should be kept below 80 mA (typ.) to remain below the PFM/PWM threshold and avoid device shutdown.
All three switchers require an input capacitor and an output inductor-capacitor filter. These components are critical to the performance of the device. All three switchers are internally compensated and do not require external components to achieve stable operation. The output voltages of the bucks can be programmed through the SPI pins.
There are several design considerations related to the selection of output inductors and capacitors:
The device has been optimized for use with nominal LC values as shown in the Typical Application Circuit.
The recommended inductor values are shown in Typical Application Diagram. It is important to ensure the inductor core does not saturate during any foreseeable operational situation. The inductor should be rated to handle the peak load current plus the ripple current:
Care should be taken when reviewing the different saturation current ratings that are specified by different manufacturers. Saturation current ratings are typically specified at 25°C, so ratings at maximum ambient temperature of the application should be requested from the manufacturer.
There are two methods to choose the inductor saturation current rating:
The best way to ensure the inductor does not saturate is to choose an inductor that has saturation current rating greater than the maximum device current limit, as specified in the Electrical Characteristics tables. In this case the device will prevent inductor saturation by going into current limit before the saturation level is reached.
If the recommended approach cannot be used care must be taken to ensure that the saturation current is greater than the peak inductor current:
where
ISAT may not be exceeded during any operation, including transients, startup, high temperature, worst-case conditions, etc.
The designer should choose the inductors that best match the system requirements. A very wide range of inductors are available as regarding physical size, height, maximum current (thermally limited, and inductance loss limited), series resistance, maximum operating frequency, losses, etc. In general, smaller physical size inductors will have higher series resistance (DCR) and implicitly lower overall efficiency is achieved. Very low-profile inductors may have even higher series resistance. The designer should try to find the best compromise between system performance and cost.
VALUE (µH) | MANUFACTURER | PART NUMBER | DCR (mΩ) | CURRENT (A) | PACKAGE |
---|---|---|---|---|---|
2.2 | Murata | LQH55PN2R2NR0L | 31 | 2.5 | 2220 |
2.2 | TDK | NLC565050T-2R2K-PF | 60 | 1.3 | 2220 |
2.2 | Murata | LQM2MPN2R2NG0 | 110 | 1.2 | 806 |
2.2 | Coilcraft | LPS3015-222MLB | 110 | 2.0 | 3015 |
2.2 | Vishay | IFSC-1008AB-ER-2R2 | 90 | 2.15 | 2520 |
Special attention should be paid when selecting these components. As shown in Figure 26, the DC bias of these capacitors can result in a capacitance value that falls below the minimum value given in the recommended capacitor specifications table. Note that the graph shows the capacitance out of spec for the 0402 case size capacitor at higher bias voltages. It is therefore recommended that the capacitor manufacturers’ specifications for the nominal value capacitor are consulted for all conditions, as some capacitor sizes (for example, 0402) may not be suitable in the actual application.
The ceramic capacitor’s capacitance can vary with temperature. The capacitor type X7R, which operates over a temperature range of −55°C to 125°C, will only vary the capacitance to within ±15%. The capacitor type X5R has a similar tolerance over a reduced temperature range of −55°C to 85°C. Many large value ceramic capacitors, larger than 1 µF are manufactured with Z5U or Y5V temperature characteristics. Their capacitance can drop by more than 50% as the temperature varies from 25°C to 85°C. Therefore X7R is recommended over Z5U and Y5V in applications where the ambient temperature will change significantly above or below 25°C.
Tantalum capacitors are less desirable than ceramic for use as output capacitors because they are more expensive when comparing equivalent capacitance and voltage ratings in the 0.47 µF to 44 µF range. Another important consideration is that tantalum capacitors have higher ESR values than equivalent size ceramics. This means that while it may be possible to find a tantalum capacitor with an ESR value within the stable range, it would have to be larger in capacitance (which means bigger and more costly) than a ceramic capacitor with the same ESR value. It should also be noted that the ESR of a typical tantalum will increase about 2:1 as the temperature goes from 25°C down to −40°C, so some guard band must be allowed.
The output capacitor of a switching converter absorbs the AC ripple current from the inductor and provides the initial response to a load transient. The ripple voltage at the output of the converter is the product of the ripple current flowing through the output capacitor and the impedance of the capacitor. The impedance of the capacitor can be dominated by capacitive, resistive, or inductive elements within the capacitor, depending on the frequency of the ripple current. Ceramic capacitors have very low ESR and remain capacitive up to high frequencies. Their inductive component can usually be neglected at the frequency ranges at which the switcher operates.
The output-filter capacitor smooths out the current flow from the inductor to the load and helps maintain a steady output voltage during transient load changes. It also reduces output voltage ripple. These capacitors must be selected with sufficient capacitance and low enough ESR to perform these functions.
Note that the output voltage ripple increases with the inductor current ripple and the Equivalent Series Resistance of the output capacitor (ESRCOUT). Also note that the actual value of the capacitor’s ESRCOUT is frequency and temperature dependent, as specified by its manufacturer. The ESR should be calculated at the applicable switching frequency and ambient temperature.
Output ripple can be estimated from the vector sum of the reactive (capacitance) voltage component and the real (ESR) voltage component of the output capacitor where:
where:
where
The device is designed to be used with ceramic capacitors on the outputs of the buck regulators. The recommended dielectric type of these capacitors is X5R, X7R, or of comparable material to maintain proper tolerances over voltage and temperature. The recommended value for the output capacitors is 22 μF, 6.3V with an ESR of 2 mΩ or less. The output capacitors need to be mounted as close as possible to the output/ground pins of the device.
MODEL | TYPE | VENDOR | VOLTAGE RATING (V) | CASE SIZE |
---|---|---|---|---|
08056D226MAT2A | Ceramic, X5R | AVX Corporation | 6.3 | 0805, (2012) |
C0805L226M9PACTU | Ceramic, X5R | Kemet | 6.3 | 0805, (2012) |
ECJ-2FB0J226M | Ceramic, X5R | Panasonic - ECG | 6.3 | 0805, (2012) |
JMK212BJ226MG-T | Ceramic, X5R | Taiyo Yuden | 6.3 | 0603, (1608) |
C2012X5R0J226M | Ceramic, X5R | TDK Corporation | 6.3 | 0603, (1608) |
There are 3 buck regulators in the LM10506 device. Each of these buck regulators has its own input capacitor which should be located as close as possible to their corresponding SWx_VIN and SWx_GND pins, where x designates Buck 1, 2, or 3. The 3 buck regulators operate at 120° out of phase, which means that they switch on at equally spaced intervals, in order to reduce the input power rail ripple. It is recommended to connect all the supply/ground pins of the buck regulators, SWx_VIN to two solid internal planes located under the device. In this way, the 3 input capacitors work together and further reduce the input current ripple. A larger tantalum capacitor can also be located in the proximity of the device.
The input capacitor supplies the AC switching current drawn from the switching action of the internal power FETs. The input current of a buck converter is discontinuous, so the ripple current supplied by the input capacitor is large. The input capacitor must be rated to handle both the RMS current and the dissipated power.
The input capacitor must be rated to handle this current:
The power dissipated in the input capacitor is given by:
The device is designed to be used with ceramic capacitors on the inputs of the buck regulators. The recommended dielectric type of these capacitors is X5R, X7R, or of comparable material to maintain proper tolerances over voltage and temperature. The minimum recommended value for the input capacitor is 10 µF with an ESR of 10 mΩ or less. The input capacitors need to be mounted as close as possible to the power/ground input pins of the device.
The input power source supplies the average current continuously. During the PFET switch on-time, however, the demanded di/dt is higher than can be typically supplied by the input power source. This delta is supplied by the input capacitor.
A simplified “worst case” assumption is that all of the PFET current is supplied by the input capacitor. This will result in conservative estimates of input ripple voltage and capacitor RMS current.
Input ripple voltage is estimated as follows:
where
This capacitor is exposed to significant RMS current, so it is important to select a capacitor with an adequate RMS current rating. Capacitor RMS current estimated as follows:
where
If any function is not used in the end application then the following recommendations for tying-off the associated pins on the circuit boards should be used.
FUNCTION | PIN | IF UNUSED |
---|---|---|
BUCK1 | VIN_B1 | Connect to VIN |
SW_B1 | Connect to VIN | |
FB_B1 | Connect to GND | |
BUCK2 | VIN_B2 | Connect to VIN |
SW_B2 | Connect to VIN | |
FB_B2 | Connect to GND | |
BUCK3 | VIN_B3 | Connect to VIN |
SW_B3 | Connect to VIN | |
FB_B3 | Connect to GND | |
SPI | SPI_CS | Connect to VIN_IO |
SPI_DI | Connect to GND | |
SPI_DO | Connect to GND | |
SPI_CK | Connect to GND | |
HL_B2 | Connect to GND | |
HL_B3 | Connect to VIN | |
STANDBY | Connect to GND | |
RESET | Connect to VIN_IO | |
COMPARATOR | VCOMP | Connect to VIN |
IRQ | Leave open |
VIN = 5 V | VOUT = 3 V |
VIN = 5 V | VOUT = 1.8 V and 3 V |