SNVS671F February 2011 – May 2019 LM21212-1
PRODUCTION DATA.
PIN | DESCRIPTION | |
---|---|---|
NO. | NAME | |
1 | SYNC | Frequency synchronization input pin. Applying a clock signal to this pin will force the device to switch at the clock frequency. If left unconnected, the frequency will default to 1 MHz. |
2 | SS/TRK | Soft-start control pin. An internal 2-µA current source charges an external capacitor connected between this pin and AGND to set the output voltage ramp rate during startup. This pin can also be used to configure the tracking feature. |
3 | EN | Active high enable input for the device. If not used, the EN pin can be left open, which goes high due to an internal current source. |
4 | AVIN | Analog input voltage supply that generates the internal bias. It is recommended to connect PVIN to AVIN through a low pass RC filter to minimize the influence of input rail ripple and noise on the analog control circuitry. |
5,6,7 | PVIN | Input voltage to the power switches inside the device. These pins should be connected together at the device. Place a low ESR input capacitance as close as possible to these pins. |
8,9,10 | PGND | Power ground pins for the internal power switches. |
11-16 | SW | Switch node pins. These pins should be tied together locally and connected to the filter inductor. |
17 | PGOOD | Open-drain power good indicator. |
18 | COMP | Compensation pin is connected to the output of the voltage loop error amplifier. |
19 | FB | Feedback pin is connected to the inverting input of the voltage loop error amplifier. |
20 | AGND | Quiet analog ground for the internal reference and bias circuitry. |
EP | Exposed Pad | Exposed metal pad on the underside of the package with an electrical and thermal connection to PGND. TI recommends connecting this pad to the PC board ground plane in order to improve thermal dissipation. |