PCB layout is critical for good power supply design. There are several paths that conduct high slew-rate currents or voltages that can interact with transformer leakage inductance or parasitic capacitance to generate noise and EMI or degrade the performance of the power supply.
- Bypass VIN to GND with a low-ESR ceramic
capacitor, preferably of X7R or X7S dielectric. Place CIN as close as
possible to the LM25183 VIN and GND pins. Ground return paths for the input
capacitor or capacitors must consist of localized top-side planes that connect
to the GND pin and exposed PAD.
- Minimize the loop area formed by the input capacitor connections and the VIN and GND pins.
- Locate the transformer close to the SW pin. Minimize the area of the SW trace or plane to prevent excessive e-field or capacitive coupling.
- Minimize the loop area formed by the diode-Zener clamp circuit connections and the primary winding terminals of the transformer.
- Minimize the loop area formed by the flyback rectifying diode, output capacitor, and the secondary winding terminals of the transformer.
- Tie the GND pin directly to the DAP under the device and to a heat-sinking PCB ground plane.
- Use a ground plane in one of the middle layers as a noise shielding and heat dissipation path.
- Have a single-point ground connection to the plane. Route the return connections for the reference resistor, soft start, and enable components directly to the GND pin. This prevents any switched or load currents from flowing in analog ground traces. If not properly handled, poor grounding results in degraded load regulation or erratic output voltage ripple behavior.
- Make VIN+, VOUT+, and ground bus connections short and wide. This reduces any voltage drops on the input or output paths of the converter and maximizes efficiency.
- Minimize trace length to the FB pin. Locate the feedback resistor close to the FB pin.
- Locate components RSET, RTC, and CSS as close as possible to their respective pins. Route with minimal trace lengths.
- Place a capacitor between input and output return connections to route common-mode noise currents directly back to their source.
- Provide adequate heatsinking for the LM25183 to keep the junction temperature below 150°C. For operation at full rated load, the top-side ground plane is an important heat-dissipating area. Use an array of heat-sinking vias to connect the DAP to the PCB ground plane. If the PCB has multiple copper layers, connect these thermal vias to inner-layer ground planes. The connection to VOUT+ provides heatsinking for the flyback diode.