SNVS118F december 1999 – may 2023 LM2594 , LM2594HV
PRODUCTION DATA
Selecting R1 and R2, as shown in Figure 9-13.
Use Equation 1 to select the appropriate resistor values.
Select R1 to be 1 kΩ, 1%. Solve for R2 using Equation 2.
Select a value for R1 between 240 Ω and 1.5 kΩ using Equation 3. The lower resistor values minimize noise pickup in the sensitive feedback pin. (For the lowest temperature coefficient and the best stability with time, use 1% metal film resistors.)
R2 = 1 k (16.26 − 1) = 15.26 k, closest 1% value is 15.4 kΩ
R2 = 15.4 kΩ