SNVS069E February 2000 – January 2022 LM2767
PRODUCTION DATA
The output characteristics of this circuit can be approximated by an ideal voltage source in series with a resistance. The voltage source equals 2 V+. The output resistance Rout is a function of the ON resistance of the internal MOSFET switches, the oscillator frequency, and the capacitance and ESR of C1 and C2. Because the switching current charging and discharging C1 is approximately twice the output current, the effect of the ESR of the pumping capacitor C1 is multiplied by four in the output resistance. The output capacitor C2 is charging and discharging at a current approximately equal to the output current, therefore, its ESR only counts once in the output resistance. A good approximation of Rout is:
where
The peak-to-peak output voltage ripple is determined by the oscillator frequency as well as the capacitance and ESR of the output capacitor C2:
High capacitance, low ESR capacitors can reduce both the output resistance and the voltage ripple.
The Schottky diode D1 is only needed to protect the device from turning on its own parasitic diode and potentially latching up. During start-up, D1 also quickly charges up the output capacitor to VIN minus the diode drop thereby decreasing the start-up time. Therefore, the Schottky diode D1 must have enough current carrying capability to charge the output capacitor at start-up, as well as a low forward voltage to prevent the internal parasitic diode from turning on. A Schottky diode like 1N5817 can be used for most applications. If the input voltage ramp is less than 10 V/ms, a smaller Schottky diode like MBR0520LT1 can be used to reduce the circuit size.