For best operational performance of
the device, use good PCB layout practices, including:
- Noise can propagate into analog
circuitry through the power pins of the circuit as a whole, as well as the
operational amplifier. Bypass capacitors are used to reduce the coupled noise by
providing low-impedance power sources local to the analog circuitry.
- Connect low-ESR, 0.1µF
ceramic bypass capacitors between each supply pin and ground, placed as
close to the device as possible. A single bypass capacitor from V+ to
ground is applicable for single-supply applications.
- Separate grounding for analog and
digital portions of circuitry is one of the simplest and most-effective methods
of noise suppression. One or more layers on multilayer PCBs are usually devoted
to ground planes. A ground plane helps distribute heat and reduces EMI noise
pickup. Make sure to physically separate digital and analog grounds, paying
attention to the flow of the ground current.
- To reduce parasitic coupling, run
the input traces as far away from the supply or output traces as possible. If
it is not possible to keep the traces separate, it is better to cross the
sensitive trace perpendicular as opposed to in parallel with the noisy
trace.
- Place the external components as
close to the device as possible. Keeping RF and RG close
to the inverting input minimizes parasitic capacitance, as shown in Figure 8-3.
- Keep the length of input traces
as short as possible. Always remember that the input traces are the most
sensitive part of the circuit.
- Consider a driven, low-impedance
guard ring around the critical traces. A guard ring can significantly reduce
leakage currents from nearby traces that are at different potentials.