SNVS515I September 2007 – January 2018 LM3102
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The LM3102 device is designed to operate from an input voltage supply range between 4.5 V and 42 V. This input supply should be well regulated and able to withstand maximum input current and maintain a stable voltage. The resistance of the input supply rail should be low enough that an input current transient does not cause a high enough drop at the LM3102 supply voltage that can cause a false UVLO fault triggering and system reset. If the input supply is more than a few inches from the LM3102, additional bulk capacitance may be required in addition to the ceramic bypass capacitors. The amount of bulk capacitance is not critical, but a 47-μF or 100-μF electrolytic capacitor is a typical choice.