SNVSB96 July 2019 LM3424-Q1
PRODUCTION DATA.
The switching frequency of the LM3424-Q1 is programmed using an external resistor (RT) connected from the RT pin to GND as shown in Figure 35.
Alternatively, an external PWM signal can be applied to the RT pin through a filter (RFLT and CFLT) and an AC-coupling capacitor (CAC) to synchronize the part to an external clock as shown in Figure 35. If the external PWM signal is applied at a frequency higher than the base frequency set by the RT resistor, the internal oscillator is bypassed and the switching frequency becomes the synchronized frequency. The external synchronization signal should have a pulse width of 100 ns, an amplitude between 3 V and 6 V, and be AC coupled to the RT pin with a ceramic capacitor (CAC = 100 pF). A 10-MHz RC filter (RFLT = 150 Ω and CFLT = 100 pF) should be placed between the PWM signal and CAC to eliminate unwanted high frequency noise from coupling into the RT pin.
The switching frequency is defined:
See the Typical Characteristics section for a plot of RT vs. fSW.