SNVS603D August 2009 – July 2019 LM3424
PRODUCTION DATA.
PWM dimming can be performed several ways:
Method 1: Connect the dimming MOSFET (Q3) with the drain to the nDIM pin and the source to GND. Apply an external PWM signal to the gate of QDIM. A pull down resistor may be necessary to properly turn off Q3.
Method 2: Connect the anode of a Schottky diode to the nDIM pin. Apply an external inverted PWM signal to the cathode of the same diode.
The DDRV pin should be connected to the gate of the dimFET with or without level-shifting circuitry as described in the PWM Dimming section. The dimFET should be rated to handle the average LED current and the nominal output voltage.