SNVS656D September 2010 – October 2016 LM3492 , LM3492-Q1
PRODUCTION DATA.
The layout of the printed-circuit board is critical to optimize the performance of the LM3492/-Q1 device application circuit. In general, external components should be placed as close to the device and each other as possible to make copper traces short and direct. In particular, components of the boost converter CIN, L1, D1, COUT, and the LM3492/-Q1 device should be closed. Also, the output feedback capacitor CFB should be closed to the output capacitor COUT. The ground plane connecting the GND, PGND, and LGND pins and the exposed pad of the device and the ground connection of the CIN and COUT should be placed on the same copper layer.
Good heat dissipation helps optimize the performance of the device. The ground plane should be used to connect the exposed pad of the device, which is internally connected to the device die substrate. The area of the ground plane should be extended as much as possible on the same copper layer around the device. Using numerous vias beneath the exposed pad to dissipate heat of the device to another copper layer is also a good practice.