SNVS598B August 2010 – March 2018 LM3535
PRODUCTION DATA.
The LM3535 can drive 8 LEDs at 25 mA each (GroupA , GroupB, GroupC) from an input voltage as low as 3.2 V, as long as the LEDs have a forward voltage of 3.6 V or less (room temperature).
The statement above is a simple example of the LED drive capability of the LM3535. The statement contains the key application parameters that are required to validate an LED-drive design using the LM3535: LED current (ILEDx), number of active LEDs (Nx), LED forward voltage (VLED), and minimum input voltage (VIN-MIN).
Equation 5 and Equation 6 can be used to estimate the maximum output current capability of the LM3535:
IADDITIONAL is the additional current that could be delivered to the other LED groups.
ROUT – Output resistance. This parameter models the internal losses of the charge pump that result in voltage droop at the pump output VOUT. Since the magnitude of the voltage droop is proportional to the total output current of the charge pump, the loss parameter is modeled as a resistance. The output resistance of the LM3535 is typically 2.4 Ω (VIN = 3.6 V, TA = 25°C) — see Equation 7:
kHR – Headroom constant. This parameter models the minimum voltage required to be present across the current sinks for them to regulate properly. This minimum voltage is proportional to the programmed LED current, so the constant has units of mV/mA. The typical kHR of the LM3535 is 4mV/mA — see Equation 8:
Equation 5 is obtained from combining Equation 7 (the ROUT equation) with Equation 8 (the kHRx equation) and solving for ILEDx. Maximum LED current is highly dependent on minimum input voltage and LED forward voltage. Output current capability can be increased by raising the minimum input voltage of the application, or by selecting an LED with a lower forward voltage. Excessive power dissipation may also limit output current capability of an application.