SNVS250F November 2004 – February 2016 LM3670
PRODUCTION DATA.
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NUMBER | NAME | ||
1 | VIN | Power | Power supply input. Connect to the input filter capacitor ( Typical Application: Fixed Output). |
2 | GND | Ground | Ground pin. |
3 | EN | Digital | Enable input. |
4 | FB | Analog | Feedback analog input. Connect to the output filter capacitor (Typical Application: Fixed Output). |
5 | SW | Analog | Switching node connection to the internal PFET switch and NFET synchronous rectifier. Connect to an inductor with a saturation current rating that exceeds the 750-mA maximum switch peak current limit specification. |