SNVS434M July 2006 – November 2016 LM3673
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The LM3673 is designed for powering low-voltage circuits from a single Li-Ion cell battery and input-voltage rails from 2.7 V to 5.5 V. The device is internally powered from the VIN pin, and the typical switching frequency is 2 MHz. The LM3673 is available in 1.2-V, 1.5-V, and 1.8-V options. An externally adjustable version is also available where the output voltage can be set with an external resistor divider to the FB pin.
For typical step-down DC-DC converter applications, use the parameters listed in Table 1.
DESIGN PARAMETER | EXAMPLE VALUE |
---|---|
Minimum input voltage | 2.7 V |
Output voltage | several fixed options; adjustable |
Maximum load current | 350 mA |
Switching frequency | 2 MHz (typical) |
The output voltage of the adjustable device can be programmed through the resistor network connected from VOUT to FB, then to GND. VOUT is adjusted to make the voltage at FB equal to 0.5 V. The resistor from FB to GND (R2) must be 200 kΩ to keep the current drawn through this network well below the 16-µA quiescent current level (PFM mode) but large enough that it is not susceptible to noise. If R2 is 200 kΩ, and VFB is 0.5 V, the current through the resistor feedback network is 2.5 µA. The output voltage of the adjustable device ranges from 1.1 V to 3.3 V.
The formula for output voltage selection is:
where
For any output voltage greater than or equal to 1.1 V, a zero must be added around 45 kHz for stability. The formula for calculation of C1 is:
For output voltages higher than 2.5 V, a pole must be placed at 45 kHz as well. If the pole and zero are at the same frequency the formula for calculation of C2 is:
The formula for location of zero and pole frequency created by adding C1 and C2 is shown in Equation 5 and Equation 6. By adding C1, a zero as well as a higher frequency pole is introduced.
See Table 2.
VOUT(V) | R1(kΩ) | R2 (kΩ) | C1 (pF) | C2 (pF) | L (µH) | CIN (µF) | COUT (µF) |
---|---|---|---|---|---|---|---|
1.1 | 240 | 200 | 15 | None | 2.2 | 4.7 | 10 |
1.2 | 280 | 200 | 12 | None | 2.2 | 4.7 | 10 |
1.3 | 320 | 200 | 12 | None | 2.2 | 4.7 | 10 |
1.5 | 357 | 178 | 10 | None | 2.2 | 4.7 | 10 |
1.6 | 442 | 200 | 8.2 | None | 2.2 | 4.7 | 10 |
1.7 | 432 | 178 | 8.2 | None | 2.2 | 4.7 | 10 |
1.8 | 464 | 178 | 8.2 | None | 2.2 | 4.7 | 10 |
1.875 | 523 | 191 | 6.8 | None | 2.2 | 4.7 | 10 |
2.5 | 402 | 100 | 8.2 | None | 2.2 | 4.7 | 10 |
2.8 | 464 | 100 | 8.2 | 33 | 2.2 | 4.7 | 10 |
3.3 | 562 | 100 | 6.8 | 33 | 2.2 | 4.7 | 10 |
There are two main considerations when choosing an inductor; the inductor must not saturate, and the inductor current ripple must be small enough to achieve the desired output voltage ripple. Different saturation current rating specifications are followed by different manufacturers so attention must be given to details. Saturation current ratings are typically specified at 25°C. However, ratings at the maximum ambient temperature of application should be requested from the manufacturer. The minimum value of inductance to ensure good performance is 1.76 µH at ILIM (typical) DC current over the ambient temperature range. Shielded inductors radiate less noise and are preferred.
There are two methods to choose the inductor saturation current rating.
The saturation current must be greater than the sum of the maximum load current and the worst case average to peak inductor current. This can be written as:
where
A more conservative and recommended approach is to choose an inductor that has a saturation current rating greater than the maximum current limit of 855 mA.
A 2.2-µH inductor with a saturation current rating of at least 855 mA is recommended for most applications. Resistance of the inductor must be less than 0.3 Ω for good efficiency. Table 3 lists suggested inductors and suppliers. For low-cost applications, an unshielded bobbin inductor could be considered. For noise critical applications, a toroidal or shielded-bobbin inductor must be used. A good practice is to lay out the board with overlapping footprints of both types for design flexibility. This allows substitution of a low-noise shielded inductor, in the event that noise from low-cost bobbin models is unacceptable.
A ceramic input capacitor of 4.7 µF, 6.3 V is sufficient for most applications. Place the input capacitor as close as possible to the VIN pin of the device. A larger value may be used for improved input voltage filtering. Use X7R or X5R types; do not use Y5V. DC bias characteristics of ceramic capacitors must be considered when selecting case sizes like 0805 and 0603. The minimum input capacitance to ensure good performance is 2.2 µF at 3-V DC bias; 1.5 µF at 5-V DC bias including tolerances and over ambient temperature range. The input filter capacitor supplies current to the PFET switch of the LM3673 in the first half of each cycle and reduces voltage ripple imposed on the input power source. The low ESR of a ceramic capacitor provides the best noise filtering of the input voltage spikes due to this rapidly changing current. Select a capacitor with sufficient ripple current rating. The input current ripple can be calculated as:
MODEL | VENDOR | DIMENSIONS L × W × H (mm) | DCR (maximum) |
---|---|---|---|
COIL | |||
BRL2518T2R2M | Taiyo Yuden | 2.5 × 1.8 × 1.2 | 135 mΩ |
DO3314-222MX | Coilcraft | 3.3 × 3.3 × 1.4 | 200 mΩ |
LPO3310-222MX | Coilcraft | 3.3 × 3.3 × 1 | 150 mΩ |
CDRH2D14-2R2 | Sumida | 3.2 × 3.2 × 1.55 | 94 mΩ |
CHIP | |||
KSLI-2520101AG2R2 | Hitachi Metals | 2.5 × 2 × 1.0 | 115 mΩ |
LQM31PN2R2M00 | Murata | 3.2 × 1.6 × 0.95 | 220 mΩ |
LQM2HPN2R2MJ0 | Murata | 2.5 × 2 × 1.2 | 160 mΩ |
A ceramic output capacitor of 10 µF, 6.3 V is sufficient for most applications. Use X7R or X5R types; do not use Y5V. DC bias characteristics of ceramic capacitors must be considered when selecting case sizes like 0805 and 0603. DC bias characteristics vary from manufacturer to manufacturer and DC bias curves should be requested from them as part of the capacitor selection process.
The minimum output capacitance to ensure good performance is 5.75 µF at 1.8-V DC bias including tolerances and over ambient temperature range. The output filter capacitor smoothes out current flow from the inductor to the load, helps maintain a steady output voltage during transient load changes and reduces output voltage ripple. These capacitors must be selected with sufficient capacitance and sufficiently low ESR to perform these functions.
The output voltage ripple is caused by the charging and discharging of the output capacitor and by the RESR and can be calculated as:
Voltage peak-to-peak ripple due to capacitance can be expressed as follows:
Voltage peak-to-peak ripple due to ESR can be expressed as follows:
Because these two components are out of phase the root mean squared (RMS) value can be used to get an approximate value of peak-to-peak ripple.
The peak-to-peak ripple voltage, rms value can be expressed as follow:
The output voltage ripple is dependent on the inductor current ripple and the equivalent series resistance of the output capacitor (RESR).
The RESR is frequency dependent (as well as temperature dependent); make sure the value used for calculations is at the switching frequency of the device.
MODEL | TYPE | VENDOR | VOLTAGE RATING | CASE SIZE inch (mm) |
---|---|---|---|---|
4.7 µF for CIN | ||||
C2012X5R0J475K | Ceramic, X5R | TDK | 6.3 V | 0805 (2012) |
JMK212BJ475K | Ceramic, X5R | Taiyo-Yuden | 6.3 V | 0805 (2012) |
GRM21BR60J475K | Ceramic, X5R | Murata | 6.3 V | 0805 (2012) |
C1608X5R0J475K | Ceramic, X5R | TDK | 6.3 V | 0603 (1608) |
10 µF for COUT | ||||
GRM21BR60J106K | Ceramic, X5R | Murata | 6.3 V | 0805 (2012) |
JMK212BJ106K | Ceramic, X5R | Taiyo-Yuden | 6.3 V | 0805 (2012) |
C2012X5R0J106K | Ceramic, X5R | TDK | 6.3 V | 0805 (2012) |
C1608X5R0J106K | Ceramic, X5R | TDK | 6.3 V | 0603 (1608) |
VOUT = 1.2 V | L = 2.2 µH | DCR = 200 mΩ |
VOUT = 1.8 V | L = 2.2 µH | DCR = 200 mΩ |
VOUT-ADJ = 3.3 V | L= 2.2 µH | DCR = 200 mΩ |
VOUT = 1.5 V (PWM Mode) |
VOUT = 1.5 V | PFM Mode 0.5 mA to 50 mA |
VOUT = 1.5 V | L = 2.2 µH | DCR = 200 mΩ |
VOUT-ADJ = 1.1 V | L= 2.2 µH | DCR = 200 mΩ |
VOUT = 1.5 V (PWM Mode) |
VOUT = 1.5 V | PFM Mode 0.5 mA to 50 mA |