SNOSCS2D November 2013 – March 2019 LM3697
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The LM3697 features an LED short fault flag indicating one or more of the HVLED strings have experienced a short. The method for detecting a shorted HVLED strings is if the current sink is enabled and the string voltage (VOUT - VHVLED1/2/3) falls to below (VIN - 1 V) . This test must be performed on one HVLED string at a time. Performing the test with more than one current sink enabled can result in a faulty reading.
The procedure for detecting a short in an HVLED string is: