SNVS402I February 2006 – May 2021 LM5009
PRODUCTION DATA
RCL: When a current limit condition is detected, the minimum off-time set by this resistor must be greater than the maximum normal off-time that occurs at maximum VIN. Using Equation 4, the minimum on-time is 0.329 µs, yielding a maximum off-time of 2.63 µs. This value is further increased by 82 ns (to 2.72 µs), resulting from a ±25% tolerance of the on-time. This value is then increased to allow for the response time of the current limit detection loop (400 ns).
The off-time determined by Equation 5 has a ±25% tolerance, as given by Equation 10:
Using Equation 5, RCL calculates to 167 kΩ (at VFB = 2.5 V). The closest standard value is 169 kΩ.