SNVSC26 October 2022 LM5012-Q1
PRODUCTION DATA
Select a ceramic output capacitor to limit the capacitive voltage ripple at the converter output. This is the sinusoidal ripple voltage that is generated from the triangular inductor current ripple flowing into and out of the capacitor. Select an output capacitance using Equation 13 to limit the voltage ripple component to 0.5% of the output voltage.
Substituting ΔIL(nom) of 909-mA gives COUT greater than 7 μF. Considering the voltage coefficients of ceramic capacitors, a 22-µF, 25-V rated capacitor with X7R dielectric is selected.