SNVS783K January 2012 – August 2021 LM5017
PRODUCTION DATA
In a conventional buck converter the output ripple voltage is calculated as shown in Equation 27.
To limit the primary output ripple voltage ΔVOUT1 to approximately 50 mV, an output capacitor COUT1 of 1.2 µF would be required for a conventional buck.
Figure 8-6 shows the primary winding current waveform (IL1) of a Fly-Buck™ converter. The reflected secondary winding current adds to the primary winding current during the buck switch off-time. Because of this increased current, the output voltage ripple is not the same as in conventional buck converter. The output capacitor value calculated in Equation 27 should be used as the starting point. Optimization of output capacitance over the entire line and load range must be done experimentally. If the majority of the load current is drawn from the secondary isolated output, a better approximation of the primary output voltage ripple is given by Equation 28.
A standard 1-µF, 25 V capacitor is selected for this design. If lower output voltage ripple is required, a higher value should be selected for COUT1 and/or COUT2.