SNVS787I January 2012 – August 2021 LM5018
PRODUCTION DATA
The on-time for the LM5018 is determined by the RON resistor and is inversely proportional to the input voltage (VIN), resulting in a nearly constant frequency as VIN is varied over its range. The on-time for the LM5018 can be calculated using Equation 3.
See Figure 6-5. RON must be selected for a minimum on-time (at maximum VIN) greater than 100 ns, for proper operation. This requirement limits the maximum switching frequency for high VIN.