SNVSB14C April 2018 – October 2021 LM5036
PRODUCTION DATA
The auxiliary feedback ripple circuit employed is presented in Figure 7-27. Having selected appropriate values for RON in Section 8.2.2.14 and RFBx in Section 8.2.2.13, the value of Cr required can be calculated using Equation 47. For our design we have opted to use a standard value Cr = 1-nF.
Based on our target output ripple specification a value for the primary output capacitor (CAUX1 = 1-µF) was chosen in Section 8.2.2.16. The primary output ripple voltage VAUX1Cap can be calculated using Equation 94. Since the value of VAUX1Cap is already greater than 25-mV there is no danger that we will fail to meet the requirement of Equation 46. Hence the value of Rr needed to ensure stable operation is calculated using Equation 48. For our design example a value of 46.4-kΩ has been selected.
The minimum value of Cac is determined using Equation 49. The precise value of this component is not very critical and for our design example we selected a convenient value of Cac = 100-nF.