The performance of switching converters heavily
depends on the quality of the PCB layout. Poor PCB design can cause among others converter
instability, load regulation problems, noise or EMI issues. Thermal relieved connections in
the power path, for VCC or the bootstrap capacitor, must not be used as thermal relieved
connections add significant inductance.
- Place the VCC, BIAS, HB1 and HB2
capacitors close to the corresponding device pins and connect them with short and wide
traces to minimize inductance, as the capacitors carry high peak currents.
- Place CSN1, CSP1, CSN2, and CSP2 filter
resistors and capacitors close to the corresponding device pins to minimize noise coupling
between the filter and the device. Route the traces to the sense resistors RCS1
and RCS2, which are placed close to the inductor, as differential pair and
surrounded by ground to avoid noise coupling. Use Kelvin connections to the sense
resistors.
- Place the compensation network
RCOMP and CCOMP as well as the frequency setting resistor
RRT close to the corresponding device pins and connect them with short traces
to avoid noise coupling. Connect the analog ground pin AGND to these components.
- Place the ATRK resistor RATRK
(when used) close to the ATRK pin and connect to AGND.
- Note the layout of following components
is not so critical:
- Soft-start capacitor
CSS
- DLY capacitor CDLY
- ILIM/IMON resistor and capacitor
RILIM and CILIM
- CFG0, CFG1 and CFG2
resistors
- UVLO/EN resistors
- Connect the AGND and PGND pin directly to
the exposed pad (EP) to form a star connection at the device.
- Connect the device exposed pad (EP) with
several vias to a ground plane to conduct heat away.
- Separate power and signal traces and use
a ground plane to provide noise shielding.
The gate drivers incorporate short
propagation delays, automatic dead time control, and low-impedance output stages capable of
delivering high peak currents. Fast rise, fall times emake sure of rapid turn-on and
turn-off transitions of the power MOSFETs enabling high efficiency. Stray and parasitic gate
loop inductance must be minimized to avoid high ringing.
- Place the high-side and low-side MOSFETs close to the device.
- Connect the gate driver outputs HO1, HO2, LO1 and LO2 with a short trace to minimize
inductance.
- Route HO1, HO2 and SW1, SW2 to the
MOSFETs as a differential pair using the flux cancellation effect reducing the loop
area.
- Place the VOUT capacitors close to the high-side MOSFETs. Use short and wide
traces to minimize the power stage loop COUT to high-side MOSFET drain
connection to avoid high voltage spikes at the MOSFET.
- Connect the low-side MOSFET source connection with short and wide traces to the
VOUT and VI capacitors ground to minimize inductance causing high
voltage spikes at the MOSFET.
- Use copper areas for cooling at the MOSFETs thermal pads.
To spread the heat generated by the MOSFETs
and the inductor, place the inductor away from the power stage (MOSFETs). However, the
longer the trace between the inductor and the low-side MOSFET (switch node) the higher the
EMI and noise emissions. For highest efficiency, connect the inductor by wide and short
traces to minimize resistive losses.