SNVSCU2A August 2024 – August 2024 LM5137-Q1
ADVANCE INFORMATION
As mentioned previously, TI recommends using one or more of the inner PCB layers as a solid ground plane. A ground plane offers shielding for sensitive circuits and traces and also provides a quiet reference potential for the control circuitry. Connect the PGND pin of the LM5137-Q1 to the system ground plane using an array of vias under the exposed pad. Also connect the PGND copper directly to the return terminals of the input and output capacitors. The PGND nets contain noise at the switching frequency and can bounce because of load current variations. The power traces (polygons) to the power-stage components for PGND, VIN and SW1/SW2 can be restricted to one side of the ground plane. The other side of the ground plane contains much less noise and is an excellent choice for sensitive analog trace routes.