The LM5143A-Q1 high-side
and low-side gate drivers incorporate short propagation delays, adaptive dead-time
control, and low-impedance output stages capable of delivering large peak currents
with very fast rise and fall times to facilitate rapid turn-on and turn-off
transitions of the power MOSFETs. Very high di/dt can cause unacceptable ringing if
the trace lengths and impedances are not well controlled.
Minimization of stray or parasitic gate loop inductance is key to optimizing gate drive switching performance, whether it be series gate inductance that resonates with MOSFET gate capacitance or common source inductance (common to gate and power loops) that provides a negative feedback component opposing the gate drive command, thereby increasing MOSFET switching times. The following loops are important:
- Loop 2: high-side MOSFET, Q1. During
the high-side MOSFET turn-on, high current flows from the bootstrap (boot)
capacitor through the gate driver and high-side MOSFET, and back to the
negative terminal of the boot capacitor through the SW connection.
Conversely, to turn off the high-side MOSFET, high current flows from the
gate of the high-side MOSFET through the gate driver and SW, and back to the
source of the high-side MOSFET through the SW trace. Refer to loop 2 of
Figure 12-1.
- Loop 3: low-side MOSFET, Q2. During
the low-side MOSFET turn-on, high current flows from the VCC decoupling
capacitor through the gate driver and low-side MOSFET, and back to the
negative terminal of the capacitor through ground. Conversely, to turn off
the low-side MOSFET, high current flows from the gate of the low-side MOSFET
through the gate driver and GND, and back to the source of the low-side
MOSFET through ground. Refer to loop 3 of Figure 12-1.
TI strongly recommends following circuit layout guidelines when designing with high-speed MOSFET gate drive circuits.
- Connections from gate driver outputs, HO1, HO2,
HOL1, HOL2, LO1, LO2, LOL1, and LOL2 to the respective gates of the
high-side or low-side MOSFETs must be as short as possible to reduce series
parasitic inductance. Be aware that peak gate drive currents can be as high
as 4.25 A. Use 0.65-mm (25 mils) or wider traces. Use via or vias, if
necessary, of at least 0.5-mm (20 mils) diameter along these traces. Route
HO and SW gate traces as a differential pair from the LM5143A-Q1 to the high-side MOSFET, taking
advantage of flux cancellation.
- Minimize the current loop path from the VCC and
HB pins through their respective capacitors as these provide the high
instantaneous current, up to 4.25 A, to charge the MOSFET gate capacitances.
Specifically, locate the bootstrap capacitor, CBST, close to the
HB and SW pins of the LM5143A-Q1 to minimize the
area of loop 2 associated with the high-side driver. Similarly, locate the
VCC capacitor, CVCC, close to the VCC and PGND pins of the LM5143A-Q1 to minimize the area of loop 3
associated with the low-side driver.