SNVSC01 February 2023 LM5148
PRODUCTION DATA
For high-power applications that do not require accurate current-limit protection, inductor DCR current sensing is preferable. This technique provides lossless and continuous monitoring of the inductor current using an RC sense network in parallel with the inductor. Select an inductor with a low DCR tolerance to achieve a typical current limit accuracy within the range of 10% to 15% at room temperature. Components RCS and CCS in #GUID-5C613DC4-3F86-4DB5-B8EB-206BF5979FDF create a low-pass filter across the inductor to enable differential sensing of the voltage across the inductor DCR.
The voltage drop across the sense capacitor in the s-domain is given by #SNVSB294584. When the RCSCCS time constant is equal to LO/RDCR, the voltage developed across the sense capacitor, CCS, is a replica of the inductor DCR voltage and accurate current sensing is achieved. If the RCSCCS time constant is not equal to the LO/RDCR time constant, there is a sensing error as follows:
Choose the CCS capacitance greater than or equal to 0.1 μF to maintain a low-impedance sensing network, thus reducing the susceptibility of noise pickup from the switch node. Carefully observe GUID-6CFB9914-50AB-4847-9B74-DE78EA03AA6F.html#GUID-6CFB9914-50AB-4847-9B74-DE78EA03AA6F to make sure that noise and DC errors do not corrupt the current sense signals applied between the ISNS+ and VOUT pins.