SNVSCM3 June 2024 LM5171
PRODUCTION DATA
The LM5171 monitors the real time inductor current in each channel by converting the current sense voltage to small current sources at the IMON1 and IMON2 pins. These monitors can be set to monitor the inductor current which in Buck mode is output current or input current in Boost mode. By programming at the CFG pin the HS- FET inductor current cycle can be monitored to measure output current in Boost mode.