SNVSB46B September 2018 – August 2021 LM5176-Q1
PRODUCTION DATA
PIN | DESCRIPTION | ||
---|---|---|---|
NAME | HTSSOP | ||
EN/UVLO | 1 | Enable pin. For EN/UVLO < 0.4 V, the LM5176-Q1 is in a low current shutdown mode. For EN/UVLO > 1.22 V, the PWM function is enabled, provided VCC exceeds the VCC UV threshold. | |
VIN | 2 | The input supply pin to the IC. Connect VIN to a supply voltage between 4.2 V and 55 V. | |
VISNS | 3 | VIN sense input. Connect to power stage input rail. | |
MODE | 4 | 1.38 V < MODE < 2.22 V : CCM, Hiccup Enabled | (Set RMODE resistor to AGND = 93.1 kΩ) |
2.6 V < MODE < VCC: CCM, Hiccup Disabled | (Set RMODE resistor to AGND = 200 kΩ or connect to VCC) | ||
DITH | 5 | A capacitor connected between the DITH pin and AGND is charged and discharged with a current source. As the voltage on the DITH pin ramps up and down, the oscillator frequency is modulated by 10% of the nominal frequency set by the RT resistor. Grounding the DITH pin will disable the dithering feature. In the external Sync mode, the DITH pin voltage is ignored. | |
RT/SYNC | 6 | Switching frequency programming pin. An external resistor is connected to the RT/SYNC pin and AGND to set the switching frequency. This pin can also be used to synchronize the PWM controller to an external clock. | |
SLOPE | 7 | A capacitor connected between the SLOPE pin and AGND provides the slope compensation ramp for stable current mode operation in both buck and boost mode. | |
SS | 8 | Soft-start programming pin. A capacitor between the SS pin and AGND pin programs soft-start time. | |
COMP | 9 | Output of the error amplifier. An external RC network connected between COMP and AGND compensates the regulator feedback loop. | |
AGND | 10 | Analog ground of the IC | |
FB | 11 | Feedback pin for output voltage regulation. Connect a resistor divider network from the output of the converter to the FB pin. | |
VOSNS | 12 | VOUT sense input. Connect to the power stage output rail. | |
ISNS(–) ISNS(+) |
13 14 |
Input or Output Current Sense Amplifier inputs. An optional current sense resistor connected between ISNS(+) and ISNS(–) can be located either on the input side or on the output side of the converter. If the sensed voltage across the ISNS(+) and ISNS(-) pins reaches 50 mV, a slow Constant Current (CC) control loop becomes active and starts discharging the soft-start capacitor to regulate the drop across ISNS(+) and ISNS(-) to 50 mV. Short ISNS(+) and ISNS(-) together to disable this feature. | |
CSG | 15 | The negative or ground input to the PWM current sense amplifier. Connect directly to the low-side (ground) of the current sense resistor. | |
CS | 16 | The positive input to the PWM current sense amplifier | |
PGOOD | 17 | Power-Good open-drain output. PGOOD is pulled low when FB is outside a -9%/+10% regulation window around the 0.8-V VREF. | |
SW2 SW1 |
18 28 |
The boost and the buck side switching nodes respectively. | |
HDRV2 HDRV1 |
19 27 |
Output of the high-side gate drivers. Connect directly to the gates of the high-side MOSFETs. | |
BOOT2 BOOT1 |
20 26 |
An external capacitor is required between the BOOT1, BOOT2 pins and the SW1, SW2 pins respectively to provide bias to the high-side MOSFET gate drivers. | |
LDRV2 LDRV1 |
21 25 |
Output of the low-side gate drivers. Connect directly to the gates of the low-side MOSFETs. | |
PGND | 22 | Power ground of the IC. The high current ground connection to the low-side gate drivers. | |
VCC | 23 | Output of the VCC bias regulator. Connect capacitor to ground. | |
BIAS | 24 | Optional input to the VCC bias regulator. Powering VCC from an external supply instead of VIN can reduce power loss at high VIN. For VBIAS > 8 V, the VCC regulator draws power from the BIAS pin. | |
PowerPAD™ | - | The PowerPAD should be soldered to the analog ground. If possible, use thermal vias to connect to a PCB ground plane for improved power dissipation. |