SNVSCG7 November 2024 LM5190
PRODUCTION DATA
PIN | TYPE(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | ISET | I/O | Dynamic current setting pin for the constant-current operation |
2 | RT | I | Frequency programming pin. A resistor from RT to AGND sets the oscillator frequency between 100kHz and 2.2MHz and DRSS disabled. A resistor from RT to VCC sets the oscillator frequency between 100kHz and 2.2MHz and DRSS enabled. |
3 | COMP | O | Transconductance error amplifier output. Connect the compensation network from COMP to AGND. |
4 | FB | I | Connect FB to VCC during initial power on to set the output voltage to pre-programmed fixed 12V. Connect FB to AGND during initial power on to set the output voltage to pre-programmed fixed 5V. Alternatively, install a resistor divider from VOUT to AGND to set the output voltage setpoint between 0.8V and 79V. The FB regulation voltage is 0.8V. |
5 | AGND | G | Analog ground connection. Ground return for the internal voltage reference and analog circuits. |
6 | IMON/ILIM | O | Current monitor and current limit programming pin |
7 | VCC | P | VCC bias supply pin. Connect a ceramic capacitor between VCC and PGND. |
8 | PGND | G | Power ground connection pin for low-side MOSFET gate driver. |
9 | LO | P | Low-side power MOSFET gate driver output. |
10 | VIN | P | Supply voltage input source for the VCC regulator. |
11 | HO | P | High-side power MOSFET gate driver output. |
12 | SW | P | Switching node of the buck regulator and high-side gate driver return. Connect to the bootstrap capacitor, the source terminal of the high-side MOSFET, and the drain terminal of the low-side MOSFET. |
13 | CBOOT | P | High-side driver supply for bootstrap gate drive. |
14 | BIAS | P | Optional supply voltage input source for VCC regulator. This input takes over if VBIAS > 9V (typical). |
15 | PGOOD | O | Power-good pin. An open-collector output that goes low if VOUT is outside the specified regulation window. |
16 | FPWM/SYNC | I | Connect FPWM/SYNC to VCC to enable forced PWM (FPWM) mode with continuous conduction at light loads. Connect FPWM/SYNC to AGND to operate the LM5190 in diode emulation mode. FPWM/SYNC can also be used as a synchronization input to synchronize the internal oscillator to an external clock signal. |
17 | EN | I | An active-high precision input with rising threshold of 1V and hysteresis voltage of 100mV. If the EN voltage is less than 0.55V, the LM5190 is in shutdown mode. |
18 | ISNS+ | I | Current sense amplifier input. Connect this pin to the inductor side of the external current sense resistor using a low-current Kelvin connection. |
19 | VOUT | I | Output voltage sense and the current sense amplifier input. Connect VOUT to the output side of the current sense resistor. |